Limitation of liability
Caterpillar makes this platform available for sharing of information, including among independent Cat dealers, to support a better Cat customer experience. Any bench-marking is in support of providing customers competitive product and service offerings. Questions regarding a dealer app should be presented directly to the dealer owning the app. For dealer apps presented on this platform, Caterpillar is not responsible for content and use. Use of this platform is subject to compliance with applicable laws. Caterpillar reserves the right to limit or suspend access to this platform for actual or threatened compliance violations.
Screenshot
Description
zamics - your asset manager for an overview of the building sector
zamics is the digital solution for asset management on the construction site. Whether foreman, site manager or workshop management - zamics offers the right solution for construction planners. With the app, you can report availabilities and update the location of work equipment. You can plan inspection dates or maintenance work. Error-prone paper processes are completely replaced by zamics.
Who seeks shall find?
If work equipment is used on several construction sites, the administration becomes confusing very quickly. This not only results in personnel costs for the search, but also avoidable expenses for new purchases. The use of zamics helps here.
This is how it works
You equip your work equipment with a robust tracker and connect it to a digital twin. From now on you always have the most important data (test date, usage status, location) always at hand in the zamics app.
Robust trackers for identifying work equipment on site.
In addition to the zamics app, you only need the zamics tracker to identify your work equipment. Our trackers are designed for demanding use in construction: The hardware used has been tested in everyday life so that it can withstand high loads. You can get the trackers directly from zamics (contact see below).
Overview of all devices on the construction site
With the zamics app, you can always keep an eye on your work equipment via the usage status - regardless of location. In this way, you can avoid problems such as hoarding devices or unnecessary replacement costs that arise, for example, from buying or renting technology that cannot be found. Since the app has a history on the usage of your work equipment, patterns can also be recognized during use and optimized for use.
Everything at a glance - the advantages of zamics
Clarity. With the zamics app you always have all device information at a glance.
Better utilization. You save money through the efficient use of work equipment.
Robust & simple. Our app has been tested for demanding use on the construction site.
Independent of manufacturer. zamics guarantees flexibility for your entire device and machine management.
----------------------------------------------------------------------
zamics - Ihr Gerätemanager für den Überblick am Bau zamics ist die digitale Lösung für das Gerätemanagement auf der Baustelle. Ob Polier, Bauleiter oder Leitung der MTA – zamics bietet für Planer am Bau die passende Lösung. Mit der App können Sie Verfügbarkeiten melden und den Standort von Arbeitsmitteln erfassen und jederzeit einsehen. Sie können Einsatzlisten für Baustellen automatisch erstellen und Prüftermine oder Wartungsarbeiten planen. Fehleranfällige Papierprozesse werden durch zamics komplett ersetzt. Wer sucht, der findet? Wenn Arbeitsmittel auf mehreren Baustellen eingesetzt werden, wird die Verwaltung sehr schnell unübersichtlich. Dadurch entstehen nicht nur Personalkosten für die Suche, sondern auch vermeidbare Aufwendungen für Neukäufe. Hier hilft der Einsatz von zamics. So funktioniert’s Sie erfassen Ihre Arbeitsgeräte per Scan mit eines robusten Trackers. Ab sofort haben in der zamics-App die wichtigsten Daten (Prüfdatum, Einsatzstatus, Ort) in einer übersichtlichen Geräteliste immer zur Hand. Robuste Tracker zur Identifizierung der Arbeitsmittel vor Ort. Neben der zamics-App brauchen Sie nur noch den zamics-Tracker zur Erfassung Ihrer Arbeitsgeräte . Unsere Tracker sind für den anspruchsvollen Einsatz am Bau konzipiert: Die verwendete Hardware wurde im Alltag getestet, damit sie auch hohen Belastungen standhält. Die Tracker können Sie direkt bei zamics (Kontakt siehe unten) beziehen. Übersicht über alle Geräte auf der Baustelle Mit der zamics-App behalten Sie Ihre Arbeitsmittel über den Einsatzstatus immer im Blick – und das standortunabhängig. So können Sie Probleme wie das Horten von Geräten oder auch unnötige Ersatzkosten vermeiden, die beispielsweise durch das Ankaufen oder Anmieten nicht auffindbarer Technik entstehen. Da die App über eine Historie zum Einsatz Ihrer Arbeitsmittel verfügt, lassen sich auch Muster bei der Nutzung erkennen und für den Einsatz optimieren. Alles im Blick - die Vorteile von zamics Übersichtlichkeit. Mit der zamics-App haben Sie jederzeit alle Geräteinformationen auf einen Blick. Bessere Auslastung. Durch den effizienten Einsatz von Arbeitsmitteln sparen Sie bares Geld. Robust & Einfach. Unsere App ist erprobt für den anspruchsvollen Einsatz auf der Baustelle. Herstellerunabhängig. zamics garantiert Flexibilität für Ihre gesamte Geräte- und Maschinenverwaltung.
Languages
English, German, Russian